You are here: Tools > AKD into KAS > Workbench User Guide > Drive Setup for Power and Bus

Power

Drive Setup for Power and Bus

The Power screen allows you to confirm Power Bus settings. Review the data on the screen to be certain the bus voltage is at the appropriate levels you expect (approximate input line AC voltage * 1.4). The other values are the appropriate limits for over voltage and under voltage for the particular drive. You can select the under voltage fault mode to trigger either only when the drive is enabled or always.

External Regeneration on pg. 1 parameters can be set from the Regen screen.

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™